Looking for Answers about Thrive Tablet (10-inch)?

Customer Questions & Answers for
Thrive Tablet (10-inch)

Customer Questions & Answers:
1,711 Questions
 | 
838 Answers
Thrive Tablet (10-inch) Page

Questions & Answers for Thrive Tablet (10-inch)

Question

Can I use my seagate external hard drive with thrive?

asked 4 years, 9 months ago
by
Anonymous
on Thrive Tablet (10-inch)
1 answer
Answers
answer 1
Without knowing the specific type of Seagate HDD you have, I can only answer in general terms. The Thrive Tablet has a full-sized USB 2.0 port. Most hard drive are setup for FAT32; the Thrive Tablet is compatible with XFAT drives. You must first reformat the hard drive and then make the connection. Use the Toshiba File Manager supplied with the Thrive Tablet to copy/move files between the two devices. Hope this helps.
Staff Answer
answered 4 years, 9 months ago
by
toshibastaff
 - Irvine, CA
Question

is this tablet compatible with micrsoft word? or office?

asked 4 years, 9 months ago
by
tabletwanter
on Thrive Tablet (10-inch)
1 answer
Answers
answer 1
Yes. The Thrive Tablet comes preinstalled with QuickOffice which allows you to READ Microsoft Word documents, Excel spreadsheets, and Powerpoint presentations. In order to create/edit documents, you need to upgrade to an application with editing capabilities. Two examples of this type of app include QuickOffice Pro HD and Documents-to-Go. Both are offered through Android Market.
Staff Answer
answered 4 years, 9 months ago
by
toshibastaff
 - Irvine, CA
Question

Will the GPS function standalone? As in no cell towers, internet, etc.

asked 4 years, 10 months ago
by
Andy
on Thrive Tablet (10-inch)
1 answer
Answers
answer 1
Yes. The Thrive has a real GPS chip similar to what a Garmin or TomTom has and without wifi or cell towers, as long as it has a clear view of the sky and is locked, it can determine your location with the precision of any other standard consumer GPS (you might need ot enable it in the location settings).
answered 4 years, 10 months ago
by
tz
 - metro detroit MI
Question

how can i open multiple windows, such as youtube, without the video stopping?

I want to open youtube, another tab, and maybe quickoffice, but when i do it, the video stops playing.
asked 4 years, 10 months ago
by
Anonymous
on Thrive Tablet (10-inch)
1 answer
Answers
answer 1
Android is built for multi-tasking. A system bar was added to the Honeycomb UI to make multi-tasking even easier as the user can see and tap into any of the apps they have open.

YouTube, however, doesn’t have the capability to in multiple windows – it’s one video at a time. If the user wants to leave YouTube and go into another app, YouTube will stay open (the video stops) but the video won’t play while in another app. It’s no different on the iPad.
Staff Answer
answered 4 years, 10 months ago
by
toshibastaff
 - Irvine, CA
Question

How do I transfer music from my ipod to my Thrive?

asked 4 years, 10 months ago
by
KK
on Thrive Tablet (10-inch)
1 answer
Answers
answer 1
go to itunes, press advanced, consolidate files, exit itunes, go to my music, itunes, select all files, copy and paste it to the sd card
answered 4 years, 10 months ago
by
Anonymous
Question

Can i connect to the internet with the help of usb internet device on the thrive ?

asked 4 years, 10 months ago
by
Eashan
on Thrive Tablet (10-inch)
1 answer
Answers
answer 1
Yes,

Although you will have to look for a usb internet device that has drivers available for andriod.
Most USB devices are detected by android without problems (keyboards/ Mice/ Thumb drives etc) but specials you have to make sure the device/manufacture supports android.
answered 4 years, 10 months ago
by
Dutch
 - Netherlands
Question

Can movies and big items be stored on an SD card and not the internal harddrive?

asked 4 years, 10 months ago
by
LK
 - Minnesota
on Thrive Tablet (10-inch)
1 answer
Answers
answer 1
Yes it can and should.

Only certain programs need to be installed on the base/main memory or internal storage of the Thrive.

Documents, audio or movie and such ca better be stored on the SD card.
answered 4 years, 10 months ago
by
Dutch
 - Netherlands
Question

Can the Thrive network wirelessly with my desktop to share files, print, etc.?

asked 4 years, 10 months ago
by
Sandy Bottom
 - Munster, IN
on Thrive Tablet (10-inch)
1 answer
Answers
answer 1
Yes it can if your computer is connected to the same network thru the wireless router you connect to with the Thrive.
answered 4 years, 10 months ago
by
Dutch
 - Netherlands
Question

Can the Thrive use my USB 3G aircard?

Does the Thrive come with drivers to use my Verizon 3G aircard like some inexpensive Chinese Android tablets do?
asked 4 years, 10 months ago
by
Don
 - Houston
on Thrive Tablet (10-inch)
1 answer
Answers
answer 1
No Tablet and specially HONEYCOMB is designed to decipher various 3G USB softwares. To read 3G Data card, software is needed. These FULL size USB are designed to read storage devices only and not application based/software based devices. So 3G data card cannot be read by THRIVE
answered 4 years, 9 months ago
by
Hunky007
Question

Does the thrive tablet have Corning gorilla glass?

asked 4 years, 10 months ago
by
Anonymous
on Thrive Tablet (10-inch)
1 answer
Answers
answer 1
No it doesn't
answered 4 years, 10 months ago
by
florida416
 - FL
<<prev 1 ... 5 6 7 8 9 ... 172 next>>
Thrive Tablet (10-inch) Page