Looking for Answers about Tecra R850?

Customer Questions & Answers for
Tecra R850

Customer Questions & Answers:
27 Questions
 | 
20 Answers
Tecra R850 Page

Questions & Answers for Tecra R850

Question

Is it possible to have the Tecra with SSD and LightScribe

I do some travelling in my proffession and would like to have a LapTop whith SSD because I have learned that SSD starts up faster than regular HD, and draws less power and thus prolongs battery-time. Further I now have to use external DVD-burner since I produce some DVD´s for my customers and I have found that the best way to label DVD's is with LightScribe, it gives a profesional look and is not easily removed.

Thank you
asked 4 years, 8 months ago
by
Noxin
 - Sweden
on Tecra R850
0 answers
Answers
This question currently has no approved answers.
Question

Is there any bios update to enable SATA III for nowdays SSD?

By default this laptop comes with SATA II although its chiptset supports SATA III. This is disabled from bios, so is there any updates to enable it?
asked 4 years, 8 months ago
by
Laurentiu
 - USA
on Tecra R850
0 answers
Answers
This question currently has no approved answers.
Question

Does the R850 an R840 come with a 9 pin serial Port?

asked 4 years, 8 months ago
by
Anonymous
on Tecra R850
1 answer
Answers
answer 1
I have the same question ! Is there a
Sub D9 serial port available?

When does Toshiba make laptops with the serial port again?

BJ
answered 4 years, 5 months ago
by
Anonymous
Question

how to connect 4 monitors?

how to connect 4 monitors using the port replicator?
asked 4 years, 8 months ago
by
softer
 - USA
on Tecra R850
0 answers
Answers
This question currently has no approved answers.
Question

How to run 4 monitors ?

The Info Page on the R850, says up to 4 displays.. How can one do that ?
asked 4 years, 8 months ago
by
Anonymous
 - Florida
on Tecra R850
0 answers
Answers
This question currently has no approved answers.
Question

does this laptop come with a vga port - 15 pin

asked 4 years, 9 months ago
by
skm
on Tecra R850
2 answers
Answers
answer 1
Yes, a display port + a VGA 15 pin port.
answered 4 years, 8 months ago
by
softer
 - USA
answer 2
Yes. All Tecra R850 models have an RGB port.
Staff Answer
answered 4 years, 8 months ago
by
toshibastaff
 - Irvine, CA
Question

Does USB 2.0 work with the USB 3 ports?

asked 4 years, 10 months ago
by
Anonymous
on Tecra R850
1 answer
Answers
answer 1
Yes. USB 2.0 devices work when using a USB 3.0 port.
Staff Answer
answered 4 years, 9 months ago
by
toshibaproductmarketing
 - Irvine, CA
Question

Does this model Tecra R850 comes with an internal modem?

asked 4 years, 10 months ago
by
Anonymous
on Tecra R850
1 answer
Answers
answer 1
Sorry, no internal modem. However, a third party USB-to-RJ11 adapter should do the trick. Here is an example: http://us.toshiba.com/accessory/309...
Staff Answer
answered 4 years, 10 months ago
by
toshibastaff
 - Irvine, CA
Question

Which of these laptop models come with support for up to 4 displays?

asked 4 years, 10 months ago
by
Jay
 - Maryland
on Tecra R850
2 answers
Answers
answer 1
I have the High Speed port replicator, but when I try to enable the 3rd monitor it doesn't work!

Only 2 at a time, either lcd panel, and a monitor or two external monitors!

How can I enable all 4 ?
answered 4 years, 3 months ago
by
Lau
 - Florida
answer 2
The models that are configured with the AMD Radeon HD 6450M graphics can support up to 4 screens. However, in order to use the 4th screen, you will need to connect to the Toshiba Hi-Speed Port Replicator II.
Staff Answer
answered 4 years, 10 months ago
by
toshibaproductmarketing
 - Irvine, CA
Question

does the laptop come with a serial port?

asked 4 years, 10 months ago
by
greg
on Tecra R850
1 answer
Answers
answer 1
Unfortunately, the Tecra R850 does not come with a serial port. However, the Toshiba Hi-Speed Port Replicator II (which the Tecra R850 can dock to) does come with a 9-pin serial port.
Staff Answer
answered 4 years, 10 months ago
by
toshibaproductmarketing
 - Irvine, CA
<<prev 1 2 3 next>>
Tecra R850 Page