Looking for Answers about NB200?

Customer Questions & Answers for
NB200

Customer Questions & Answers:
433 Questions
 | 
452 Answers
NB200 Page

Questions & Answers for NB200

Question

Is that 160gb hdd compatible with sata II interface?

I'd like to switch traditional hard drive with a fast 2'5 ssd.
asked 3 years, 10 months ago
by
markowski_85
on NB200
1 answer
Answers
answer 1
This netbook uses the same chipset as every other Atom-based netbook - the Mobile 945 chipset. You can plug in an SSD drive and it'll work just fine, but I'm pretty sure the 945 chipset only supports SATA I transfer rates.
answered 3 years, 10 months ago
by
gaz
 - southern california, united states
Question

How many Amps does the NB205-N210 use?

Plan to power the mini in auto with 400Watt inverter made by Black & Decker. It will provide up to 3.48 Amps.
Is this sufficient power for the mini?
asked 3 years, 10 months ago
by
Dave
 - Kansas
on NB200
1 answer
Answers
answer 1
Power requirement is 30W (19V @ 1.58A) - via auto sense 100-240v/50-60Hz AC power adapter
answered 3 years, 10 months ago
by
ServiceTech
Question

Can you download Office 2007 on the mini notebook?

asked 3 years, 10 months ago
by
Anonymous
on NB200
1 answer
Answers
answer 1
Yes. And it runs well.
answered 3 years, 10 months ago
by
David Garrison
 - Woodland, CA
Question

How is the speaker volume?

I have the NB205-N311 and I must say that the sound volume is extremly low.

is their a way to adjust it?
asked 3 years, 10 months ago
by
Willi
on NB200
1 answer
Answers
answer 1
There is a single small speaker, which reduces cost and power requirements, which necessarily limits the available volume. I suspect the intent is that the speaker is merely there for system sounds, attention 'dings', etc., and that music listening, voip, or gaming is done with headphones or external speakers. I have been using a competitor's netbook for some time and, even thought the unit's stereo speakers are quite good, in real-world use, I find myself using headphones most of the time. Although somewhat disappointing, I think this is a reasonable design decision.
answered 3 years, 10 months ago
by
Slipstick
Question

Does this laptop also have a microphone for video chatting?

asked 3 years, 10 months ago
by
Anonymous
on NB200
1 answer
Answers
answer 1
Yes, there is a built-in mic. If you use the zoom tool on our photo gallery, you can clearly see it next to the webcam.

Here is a link to our photo gallery for the NB200.

http://laptops.toshiba.com/laptops/...
Staff Answer
answered 3 years, 10 months ago
by
toshibastaff
 - Irvine, CA
Question

Does this laptop works with Window Vista?

asked 3 years, 10 months ago
by
Anonymous
on NB200
1 answer
Answers
answer 1
yeah it would actually work out but the laptop would be very slow and it may work better if you use 2gigs of the ram
answered 3 years, 10 months ago
by
Gabriel
Question

SSD option?

Will there be an option to have a solid state drive instead of the standard 160gb HDD?
asked 3 years, 11 months ago
by
Anonymous
on NB200
1 answer
Answers
answer 1
Not that I know or heard of
answered 3 years, 11 months ago
by
Anonymous
Question

Does this laptop have a matte screen?

asked 3 years, 11 months ago
by
Lou
on NB200
1 answer
Answers
answer 1
10.1” 1024 x 600 Glossy LED Display
answered 3 years, 11 months ago
by
Anonymous
Question

Intel Atom Processor infos?

What processor is used for the Toshiba mini NB200?
Does the processor support x86 and x64?
Does it support hardware virtualization, if yes can the end user have the option to enable it in the bios?

Hardware virtualization is important especially for users that are planning to install Micrsoft Windows 7 and run a feature called Windows 7 XP mode.*

*Windows 7 XP mode in only available from Microsoft Windows 7 Professional and above only
asked 3 years, 11 months ago
by
Anonymous
on NB200
1 answer
Answers
answer 1
There is an Atom N280 1.66
answered 3 years, 11 months ago
by
hel
 - Montreal
Question

What are my limitations with this mini versus a regular laptop?

asked 3 years, 11 months ago
by
CookieMonster
 - Delaware, DE
on NB200
1 answer
Answers
answer 1
I said the normal speaker are extremely low, so you need to buy separete speaker or use headset, but beside that you paid for what you get, size, no dvd drive, and very small screen
answered 3 years, 10 months ago
by
ray
<<prev 1 ... 5 6 7 8 9 ... 44 next>>
NB200 Page