Looking for Answers about L500?

Customer Questions & Answers for
L500

Customer Questions & Answers:
403 Questions
 | 
197 Answers
L500 Page

Questions & Answers for L500

Question

Does this laptop run windows xp?

asked 6 years, 9 months ago
by
Anonymous
on L500
1 answer
Answers
answer 1
yes
run windows xp is very good
answered 6 years, 9 months ago
by
fliming
 - china
Question

shall we change the processor

asked 6 years, 9 months ago
by
murali
on L500
1 answer
Answers
answer 1
Processors on Toshiba laptops are not socketed and so cannot be changed.
Staff Answer
answered 6 years, 9 months ago
by
toshibastaff
 - Irvine, CA
Question

Does this laptop have additional number pad

asked 6 years, 9 months ago
by
Anonymous
on L500
1 answer
Answers
answer 1
It depends on the screen size. The larger sizes do, the smaller don't.
answered 6 years, 9 months ago
by
Anonymous
Question

Does this laptop have a scroll button on the mouse?

I haven't been able to find one and it's exceedingly annoying! On my old laptop clicking both mouse buttons at the same time brought up a scroll button and on Macs you can use two fingers to scroll. This doesn't seem to have any, and you therefore have to rely on the scroll bars on the right-hand side of windows - very bothersome. Could Toshiba upgrade the mouse driver to include a scroll button?
asked 6 years, 9 months ago
by
Anonymous
on L500
1 answer
Answers
answer 1
The touchpad does have a scroll bar on the right-hand side, and the bottom. However, for these to function you have to have the right driver installed. Go to downloads and download the touchpad driver. If downloading and self-extraction of the drivers does not install it, you need to extract it to a folder and run the setup application. This should make it work.
answered 6 years, 9 months ago
by
Anonymous
Question

do i HAVE AUTOMATIC SPELLCHECK WITH MY NEW LAPTOP

asked 6 years, 10 months ago
by
Anonymous
on L500
1 answer
Answers
answer 1
Automatic spellcheck usually comes with, and works within, a specific application (such as Microsoft Word). The laptop itself doesn't have it.
answered 6 years, 9 months ago
by
Anonymous
Question

How much does the L500 weight?

It might help the consumer if Toshiba publishs the laptop weight's in the Specs, like other laptop manufacturers do..
asked 6 years, 10 months ago
by
Kishor
 - Raleigh, NC
on L500
1 answer
Answers
answer 1
Toshiba does publish laptop weight. Since it varies by configuration, you will find it located on the model page under Weight in the Detail Product Specs portion of the page, or in the Detailed Spec PDF attached to the page under the Physical Description section.

There are three screen sizes associated with the L500 Series. Weight will vary accordingly:
- L500/L505 (16-inch): Starting at 6.0 lbs.
- L515 (14-inch): Starting at 5.07 lbs.
- L550/L555 (17.3-inch): Starting at 6.99lbs.
Staff Answer
answered 6 years, 9 months ago
by
toshibastaff
 - Irvine, CA
Question

does the wireless adapter have multiple antennas (MIMO divesity - 802.11n-draft technology)?

asked 6 years, 10 months ago
by
ExxAge
 - Croatia
on L500
1 answer
Answers
answer 1
Yes, Toshiba L500 laptops are equipped with two antennas to support the MIMO diversity.
Staff Answer
answered 6 years, 10 months ago
by
toshibastaff
 - Irvine, CA
Question

what is the bridge media adapter slot for

asked 6 years, 10 months ago
by
Anonymous
on L500
1 answer
Answers
answer 1
The Bridge Media Adapter, also known as the Memory Card Reader, comes standard on all Satellite L500 models. It also you to read/write data from a variety of compatible memory cards to/from the hard drive.

Below are the compatible formats for this series: Secure Digital, Secure Digital High Capacity, Mini SD, Micro SD, Memory Stick™, Memory Stick PRO™, Multi Media Card [shared
slot].
Staff Answer
answered 6 years, 10 months ago
by
toshibastaff
 - Irvine, CA
Question

data on L505D S6952 memory

asked 6 years, 10 months ago
by
Anonymous
on L500
1 answer
Answers
answer 1
The Satellite L505D-S6952 comes with 4GB 800MHz memory standard, expandable to 8GB. For a complete list of specifications, please refer to the link below:

http://cdgenp01.csd.toshiba.com/con...
Staff Answer
answered 6 years, 10 months ago
by
toshibastaff
 - Irvine, CA
Question

Does the L500 PSLJOA-01e013 qualify for the windows 7 upgrade

asked 6 years, 10 months ago
by
tonyl
 - Australia
on L500
1 answer
Answers
answer 1
For information on the Toshiba Windows 7 Upgrade program offered in Australia, please refer to the link below:

http://www.isd.toshiba.com.au/windo...
Staff Answer
answered 6 years, 10 months ago
by
toshibastaff
 - Irvine, CA
<<prev 1 ... 12 13 14 15 16 ... 41 next>>
L500 Page